Pour les grandes quantités et les produits personnalisés, ajoutez à votre panier et cliquez sur Demander un devis, oucontactez-nouset nous vous répondrons sous 2 jours ouvrés.
(41 Types de produit)
These Linear Guide rails are a linear motion-bearing system used to guide and support moving components in a linear direction. Linear guide rails are made up of two major components: a rail and a carriage. The rail is a long, straight beam attached to a permanent surface. The carriage is a moving block that goes along the rail. The carriage comprises bearings that make contact with the rail and offer low-friction linear motion.
These rails are used in applications requiring high accuracy, low friction and smooth movements. It can sustain dynamic loads while accounting for impact, vibration, and fatigue.
In general, the carriages will be delivered to the tracks individually. To put the carriage onto the tracks, bring it up to the rails and slide it onto the rail. It is widely utilised in high-load and accurate applications throughout the industry, including medical devices, semiconductor production equipment, and industrial automation equipment.
These Miniature Linear Rails are used to direct and support moving loads. It delivers smooth and accurate linear motion in small systems. They comprise a foundation rail, a sliding block, and a series of rolling parts. The base rail is attached to the machine frame, and the slide block slides along it. The rolling components, commonly ball bearings, sustain the weight and decrease friction between the sliding block and the base rail.
It can withstand dynamic loads while considering impact, vibration, and fatigue. As this is a precise system they must be mounted on accurately prepared surfaces.
The carriages come mounted on dummy blocks. Offer the carriage up to the rails and move it off the block and onto the rail to install it. They are often smaller and lighter than regular linear rails, making them excellent for applications requiring restricted space and weight, such as scientific applications, medical equipment, or semiconductor manufacturing.
These miniature rail carriages are a compact and versatile solution for achieving precise linear motion in small-scale applications. They're perfect for applications that need accurate placement and fluid movement in constrained places due to their small size, or applications requiring corrosion resistance as they are made from stainless steel.
The rails' 45 contact gothic arch design guarantees similar load capabilities in all directions. These rails move smoothly and feature a low coefficient of friction and break-away forces. It can sustain large weights, is resistant to corrosion, and is resilient to wear and tear.
Carriages come with a plastic dummy rail. It should be mounted by putting the dummy rail up against the end of the real rail and sliding it from one to the other. It is capable of withstanding temperatures between -40C and +80C. Used in different applications, including medical devices, pharmaceuticals, small automation systems, and optical equipment.
These Quadro Carriages are closed, with self-aligning linear ball bearings, two integrated seals, and a lubrication hole. They achieve accurate and efficient linear motion in heavy-load applications.
It features four linear ball bushings internally, which improves stability and load-bearing capability. It distributes the load uniformly throughout the carriage, minimising deflection and maximising stiffness, lowering the danger of vibration and providing dependable performance even in high-speed applications.
It can withstand temperatures ranging from 20C to +80C. However, by replacing the ball retainers, end plates, and seals it can tolerate temperatures of up to +120C. Commonly used in applications such as food packaging machines, printing machines, computers, or tool grinders.
These Rail Clamps are used in combination with rail carriages. Made to endure demanding conditions such as heavy loads or vibrations, it offers a secure and strong grip on the rails and maintains remarkable strength and longevity.
By adjusting the clamping lever, the contact sections are pressed into contact with the rail, thereby fastening the carriage in place. It has a circular motion instead of a friction coefficient, reduced driving resistance, and lower energy consumption.
Designed with specialized mechanisms, it allows for easy installation and adjustment, guaranteeing a tight and sturdy connection. Used in heavy-duty applications such as machinery, railway systems, and manufacturing applications.
These Shaft support rails are used to provide continuous support and stability for linear shafts. They are frequently used with linear bearings to provide a fully supported low friction system.
It comes with a hardened steel shaft and mounting holes to mount and support across its entire length. These rails are used with open linear bearings or carriages to create a linear motion system.
The shaft is pre-mounted to the shaft support rail. It has great durability and wear resistance, allowing it to tolerate high application loads and repetitive motion. It is widely used in industrial, automotive, medical devices, and electronics manufacturing.
Les supports d'extrémité d'arbre apportent aux arbres linéaires stabilité, alignement et soutien. Ces composants sont destinés à maintenir fermement en place des diamètres d'arbre standard tout en permettant un mouvement lisse et précis de la douille.
Ils maintiennent fermement l'arbre en place, en limitant le mouvement latéral ou radial qui pourrait provoquer un mauvais alignement ou entraîner une usure excessive. Ils sont utilisés dans les applications incluant les machines-outils, les dispositifs médicaux et les équipements d'automatisation industrielle.
These Unflanged Aluminium Carriages are a type of linear bearing that is very effective for heavy loads in various applications where they guide and support linear motion. Their rails are composed of contoured aluminium, with two hardened stainless steel shafts pressed to function as the raceways for the runner block balls.
The unflanged design provides a more compact solution when compared against the flanged carriages but the moving component in the application can only be mounted to the top of the carriage.
Because it is lighter and more corrosion-resistant than steel, it can be used in various applications, including aerospace, machinery, handling technology, machine enclosures, medical, food, etc.
These low-profile unflanged carriages are linear bearings used for heavy-duty and precise linear motion applications. They give precision, stability, and dependability. The four row contact with the mating rail offers the same load capacity capabilities regardless of the load pressing into the carriage or hanging from it.
The unflanged design provides a more compact solution but can only be mounted to from the top. The carriages' ball retainers allow for a quieter operation whilst improving lubrication of the system. It also ensures the balls remain in place should the carriage be removed from the rail in error.
Its low profile provides an even smaller compact solution when compared again the standard unflanged linear carriages. It is used in many applications, including special purpose equipment, automation, material handling systems, medical devices, etc.
These low-profile unflanged carriages are linear bearings used for heavy-duty and precise linear motion applications. They give precision, stability, and dependability. The four row contact with the mating rail offers the same load capacity capabilities regardless of the load pressing into the carriage or hanging from it.
The unflanged design provides a more compact solution but can only be mounted to from the top. The carriages' ball retainers allow for a quieter operation whilst improving lubrication of the system. It also ensures the balls remain in place should the carriage be removed from the rail in error.
The carriages are supplied on dummy blocks which must be offered up to the edge of the rail the carriage is going onto during installation. Slide the carriage from the dummy block onto the rail to ensure no damage can occur. It is used in many applications, including special purpose equipment, automation, material handling systems, medical devices, etc.
Les vis à billes sont des composants de précision utilisés dans les systèmes de mouvement linéaire pour convertir un mouvement rotatif en mouvement linéaire avec efficacité et exactitude. Elles sont composées d'un arbre (ou d'un écrou) fileté et d'un jeu de paliers à billes rectifiés avec précision. Les paliers à billes roulent entre l'arbre et l'écrou, réduisant le frottement et l'usure courants dans les systèmes de mouvement de glissement.
Ils sont couramment utilisés dans différentes applications industrielles, en particulier dans l'automobile, l'aérospatiale et les équipements médicaux. En fonction du diamètre, une large sélection de vis à billes sont disponibles.
À noter : Ne retirez pas la vis à billes du manchon avant assemblage car cela entraînerait un échappement des billes et rendrait l'écrou inutilisable.
Les vis mères sont un type de vis utilisé pour convertir un mouvement rotatif en mouvement linéaire en convertissant le mouvement rotatif de la vis en mouvement avant de l'écrou. « Mère » fait référence à la distance que parcourt un écrou pour un tour complet de la vis.
Elles sont utilisées pour les applications standard qui nécessitent un faible degré de précision et d'exactitude ou lorsqu'une vis mère n'est pas adaptée en raison des conditions environnementales. Elles sont solides, durables et plus rentables que les vis à billes. Elles sont également employées en robotique et dans les secteurs automobile et de l'usinage CNC.
Disponibles en tant que vis mères filetés main droite standard, ainsi que filetés main gauche.
Les écrous cylindriques en acier sont des fixations qui sont couramment utilisées en combinaison avec des vis mères ou des vis à billes pour convertir un mouvement rotatif en mouvement linéaire. L'écrou est fileté sur la vis et se déplace sur la longueur de la vis pendant sa rotation, fournissant un mouvement linéaire lisse et précis.
Ils sont utilisés pour des vitesses de rotation basses, un contrôle manuel et des fonctions de serrage. Ils ne sont pas adaptés aux mouvements motorisés. Ils disposent de filetages qui sont adaptés à la vis, ce qui assure une durabilité et une résistance à l'usure exceptionnelles grâce à leur matière.
Ils sont utilisés dans les secteurs de l'automobile, de l'aérospatiale ou de la construction pour maintenir les vis mères en place. Disponibles en tant qu'écrous cylindriques en acier filetés main droite standard, ainsi que filetés main gauche.
Les écrous cylindriques en bronze sont utilisés avec nos vis mères pour convertir un mouvement rotatif en mouvement linéaire. L'écrou est fileté sur la vis et se déplace sur la longueur de la vis pendant sa rotation, fournissant un mouvement linéaire lisse et précis.
Idéaux pour les applications manuelles ou motorisées à une rotation allant de lente à moyenne. Ils disposent de filetages qui sont adaptés à la vis, ce qui assure une durabilité et une résistance à l'usure exceptionnelles grâce à leur matière. Fabriqués en bronze qui possède une meilleure résistance à la corrosion que l'acier, mais est moins solide ou résistant à la chaleur.
Ils sont utilisés dans les secteurs de l'automobile, de l'aérospatiale ou de la construction pour maintenir les vis mères en place. Disponibles en tant qu'écrous cylindriques en bronze filetés main droite standard, ainsi que filetés main gauche.
Les écrous à brides en bronze constituent une partie importante des assemblages de vis mères, très utilisés dans les systèmes de mouvement linéaire. Ils sont destinés à des applications manuelles ou motorisées à des vitesses de rotation basses en charge et ils disposent d'une surface lisse qui réduit l'usure de la vis mère.
Ils sont extrêmement durables et dotés d'un élément d'auto-lubrification. Le bronze assure une performance fiable, ce qui fait d'eux un des choix d'écrous les plus populaires dans les assemblages de vis mères.
Ils sont couramment utilisés dans une variété d'applications industrielles, notamment dans l'automobile, l'aérospatiale et les équipements médicaux.
Disponibles en tant qu'écrous à brides en bronze filetés main droite standard, ainsi que filetés main gauche.
Les écrous à billes et à brides constituent un composant essentiel des assemblages de vis à billes. Ce sont des composants mécaniques de précision utilisés dans les systèmes de mouvement linéaire. Ces écrous, comme leur nom l'indique, comprennent une bride qui est un bord plat saillant qui ressort de l'écrou et offre un soutien supplémentaire et facilite l'installation.
Ils sont utilisés en combinaison avec des vis à billes pour convertir un mouvement rotatif en mouvement linéaire. Des paliers à billes dans l'écrou roulent le long de la vis à billes pendant qu'elle tourne, en produisant un mouvement linéaire lisse et précis. La bride dispose d'une tolérance étroite, assurant un jeu minimal, ainsi qu'une précision et une justesse élevées.
Ils sont couramment utilisés dans une variété d'applications industrielles, notamment dans l'automobile, l'aérospatiale et les équipements médicaux.
Veuillez garder à l'esprit que le retrait de l'écrou à billes du manchon fourni peut aboutir à l'échappement des paliers à billes, rendant ainsi l'écrou à billes inutilisable.
Malheureusement, votre session a expiré pour cause d'inactivité. Veuillez vous connecter à nouveau ou recharger la page pour continuer