Thermal management and cable protection for sensitive components

Thermal management application

Properly specified heat-resistant cable management can make the difference between a stable system and one that fails prematurely. And while operating temperatures create strain on assemblies, cooling measures help, but don’t address all the problems. Cable entry points, mounting hardware and routing paths all sit in the same heated environment. This guide looks at how heat affects sensitive assemblies and sets out practical engineering measures to reduce risk in demanding applications. We’ll cover:

Why thermal management matters 
Common heat risks 
Protection strategies  
Typical application for thermal management 
How to choose the components 
Conclusion and expert resources

Why thermal management matters

Electronic systems now process more power within smaller footprints. That higher power density means more heat is generated in confined spaces. Without effective thermal management solutions, temperatures rise rapidly.

Consider that elevated operating temperatures accelerate chemical and material degradation. Push components beyond their thermal rating, and their behaviour changes. Semiconductor parameters move away from nominal values. Electrolytic capacitors lose electrolyte at a faster rate. Cable insulation can stiffen, crack, or lose insulating capability.

Failure isn't always immediate, but cumulative. Components that operate just above their rated temperature tend to age faster than expected. What looks acceptable during testing can translate into reduced field life once real duty cycles are applied.

As thermal exposure continues, built in tolerance begins to shrink. Circuits become less forgiving under peak load or abnormal conditions. Minor variations in supply or environment can then trigger faults that wouldn't occur at lower temperatures.

If thermal control is overlooked, the consequences surface later as warranty returns, service interventions, or compliance concerns. That's why temperature management needs to be addressed at concept stage, particularly in demanding industrial cable management applications.

Common heat risks

Heat within an assembly is rarely uniform. Power semiconductors, transformers, and high load resistors create concentrated hot zones that expose nearby conductors to sustained thermal stress. Without properly specified heat-resistant cable management, insulation can degrade far sooner than anticipated.

Cables routed through these pockets sit in a harsher environment than the average internal temperature suggests. If heat-resistant cable management isn't considered early on, insulation conditions can deteriorate well before the expected service interval.

Equipment in service heats up. Later, it cools down again. That pattern repeats throughout its life.

Each temperature change affects the materials inside differently. Copper conductors expand. Polymer supports respond at another rate. Steel fixings behave differently again. These small variations occur within the same industrial cable management assembly.

Over time, the repeated movement begins to show. A termination secured with cable clips or clamps may lose some clamping force. Conductors can shift slightly within their routing path. What started as a stable installation gradually becomes more vulnerable, especially where heat-resistant cable management has not been properly specified.

Material behaviour also changes with heat. Some polymers lose rigidity as temperatures climb, which reduces their resistance to rubbing or vibration. In machinery with moving parts, cables can begin to fret against edges or inadequately placed cable routing hardware, wearing through protective layers.

Temperature changes also affect enclosure pressure. As air inside heats, it expands. When the unit cools, it can draw in moisture-laden air from outside. Without correctly selected cable protection components, ingress can compromise both insulation performance and long-term reliability.

Protection strategies

High temperature polymers such as PA66, TPE, and silicone retain mechanical strength and dielectric performance under sustained heat. When specified correctly, materials form the frontline for thermal management solutions.

They also influence thermal conduction. Metals readily pass heat from one part of an assembly to another. Most engineered plastics do not. When used for clips, spacers, or even screws, they interrupt that conductive path. This can reduce the amount of heat transferred from a hot panel or bracket into other components.

Smart routing is equally important. Cables should be positioned away from known hot zones and high load components. Well-designed cable routing hardware maintains separation distances and prevents unintended contact with heat sources.

Insulation and sleeving provide an additional thermal barrier. Purpose specified sleeves support heat-resistant cable management in areas where rerouting is not feasible. They also reduce the risk of abrasion in dynamic environments.

Cables need to stay where they were designed to sit. If they move, they can end up closer to a heat source than intended. Properly specified cable clips and clamps hold the intended routing in place.

Panel openings are another weak point. The raw edge of a cut out can damage insulation, particularly once materials have been exposed to heat. Fitting grommets or bushings provides a defined interface and a degree of environmental control.

Temperature changes also affect internal air pressure. As an enclosure warms, air expands. When it cools, air is drawn back in. Vent plugs manage that exchange so it does not occur through random gaps or stressed seals.

Browse our range of engineered-plastic screws


Typical applications for thermal management

In white goods, heating elements, motors, and control boards often sit within the same enclosure. They're separated only by brackets or panels.

Harness routing follows the available paths. That can mean running conductors past heater housings or along steel panels that retain heat after the cycle ends. The surrounding air temperature may be acceptable, yet the local surface temperature is much higher.

In this context, insulation is not exposed to a brief spike but to repeated operating heat. Appropriately specified heat-resistant cable management is needed to maintain electrical integrity and design clearances over the intended service life.

Our experts help you learn about your choices in Quick guide: industrial components for consumer appliances.

Heating, ventilation, and air conditioning systems have comparable constraints. Compressors and drives produce heat as a function of load. They're typically enclosed within factory-built units where the layout is fixed. Cable routes follow the available structure, not an optimised thermal plan. Proximity to warm casings and ongoing vibration from rotating parts must be accounted for at the support and fixing stage.

Commercial catering equipment and industrial machinery operate with heat as a constant. Cooking appliances and processing plants are intended to remain at working temperature for extended periods. Adjacent panels and support frames absorb that heat and do not cool immediately when the cycle ends. Component selection in these environments is based on sustained exposure, not short duration events.

How to choose the components

Begin with temperature rating. Materials must withstand the maximum continuous operating temperature, not just nominal conditions. This applies to fixings, insulation, and enclosure interfaces within any industrial cable management system.
 

cable clamps

When choosing cable clips and clamps, check how they behave at the temperatures they will actually see. Some plastics lose stiffness as they warm, which affects grip. If the operating temperature is within 105°C, then standard nylon 6/6 will do. If higher, consider metal clamps.

Browse our range of cable ties and clips

Browse our range of cable clamps

Panel cut outs

Panel cut outs are a frequent weak point. The edge of stamped steel or moulded plastic can damage insulation, especially once temperatures rise.

Cable grommets and cable bushings

Choose grommets and bushings with both fit and material behaviour in mind. Under heat, some elastomers harden or lose flexibility. Others maintain resilience and continue to protect the cable from edge contact over time.
 

Browse our range of cable grommets

Browse our range of cable bushings

cable wraps and sleeves

Where conductors pass close to hot components, heat-resistant sleeving provides an additional safeguard. Sleeve material should be matched to the expected temperature profile and exposure duration. In higher risk zones, layered protection is certainly justified.

Browse our range of cable wraps & sleeves

vent plugs

Venting is often overlooked during specification. Vent plugs support pressure equalisation while limiting moisture ingress. In thermally active enclosures, they help stabilise internal conditions and reduce stress on seals.

Browse our range of vent plugs

PCB spacers

PCB standoffs also play a role in thermal resilience. Adequate board spacing improves airflow and reduces heat transfer to adjacent surfaces. Material choice influences both electrical insulation and dimensional stability at elevated temperatures. 

Browse our range of PCB spacers

You can get a deeper understanding in our Guide to PCB standoffs. 
 

Each component should be assessed as part of an integrated thermal management solutions strategy. Selecting in isolation only increases the risk of mismatch and premature failure.

At a glance: Selection criteria for thermal management

Component type

Key selection criteria

Thermal considerations

Typical risk if incorrectly specified

Cable clips & clamps

Material strength, retention force, mounting method

Derating at elevated temperatures

Loosening, cable movement, insulation wear

Grommets & bushings

Material flexibility, edge protection, fit tolerance

Resistance to hardening or cracking

Abrasion, ingress, seal failure

Heat-resistant sleeving

Continuous temp rating, flame class, thickness

Proximity to hot components

Insulation breakdown

Vent plugs

IP rating, airflow capacity, membrane type

Pressure equalisation under heat

Moisture ingress, seal stress

PCB standoffs

Material stability, height, insulation class

Airflow and heat transfer

Localised overheating

What about other components? Our experts have put together a helpful guide, What components are needed for industrial cabinets and enclosures?

Conclusion and expert resources

Thermal stress influences cable integrity, mechanical retention, sealing performance, and overall system reliability. Ignoring these interactions increases the likelihood of premature failure and costly redesign.

Effective thermal management solutions require a joined-up approach. Material selection, routing strategy, protection methods, and ventilation must work together. Well specified cable protection components ensure that conductors remain secure, insulated, and shielded from environmental exposure. In high-temperature environments, detail matters. The correct choice of cable clips, clamps, grommets, bushings, sleeving, and venting hardware directly impacts service life.

Use our expert resources to learn more: 

IET (Institution of Engineering and Technology)
Publisher of the IET Wiring Regulations (BS 7671) and Wiring Matters, offering authoritative guidance on electrical installations, thermal effects, and cable current carrying capacity.

Wiring Matters (IET Magazine)
Technical articles exploring practical aspects of cable installation, temperature derating, and system reliability.

Materials World (IOM3 magazine)
Engineering materials insight from the Institute of Materials, Minerals & Mining, helpful for polymer performance and ageing under heat. 

Download free CADs

Free CADs are available for most solutions, which you can download. If you’re not quite sure which cable protection components will work best for your application, our experts are always happy to advise you. Whatever your requirements, you can depend on fast dispatch. 

Download free CADs

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application at 0345 528 0474.